SPI issue keep getting 0 values from accelerometer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-05 10:57 AM
NUCLEO-WB55RG communicating via SPI1 to an ADXL362 eval board
I set up the project (attched below) using CubeIDE, generated the code & placed my own callbacks for the SPI in main.
When I look at the value for the Z direction I should be getting a value that indicates roughly 1g but all I get is 0. The same for all the other axis, no change in any value no matter how I orient the sensor.
To check that the acceleromter was working I hooked it up to an Arduino using a 3rd party library especially for the ADXL362. That all worked as expected, so I know the accelerometer is working.
When I go through the code with the debugger it doesn't hang anywhere so I'm guessing my callbacks are working, its just I dont get any data back, all values remain at 0
Anyone see anything obvious that I'm doing wrong?
Solved! Go to Solution.
- Labels:
-
ST boards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-07 7:36 AM
From the scope, top row is from the STM32WB55, bottom row from the Arduino.
Channel 1 - top trace is the CS line. I couldn't get a reading of the clock & the CS line one the Arduino, as soon as I probed SCLK then the chip errored out and just returned 0s & the clock & CS traces interfered with each other..
The STM MISO line is always 0 no matter what command I send, so no ID, no axis data, always 0.
I notice the CS line has that blip which I assume is the gap between bytes being sent?
SCLK is bang on 4MHz
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-07 7:55 AM
Does your scope not have a trace capture or screenshot facility?
@NicRoberts wrote:I notice the CS line has that blip which I assume is the gap between bytes being sent?
Looks like it.
That'll be (at least one reason) why it's not working - CS should stay low for the entire transaction:
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-07 8:03 AM
@Andrew Neil wrote:Does your scope not have a trace capture or screenshot facility?
It doesnt even have a USB port :D just an old school parallel port.
That'll be (at least one reason) why it's not working - CS should stay low for the entire transaction:
Yeah that's what I was expecting. I cant see it in the code unless the CS is being taken care of in the HAL & I shouldn't be setting & resetting it in my ADXL362 driver?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-07 8:10 AM
On STM32's most SPI requires you drive the CS from a GPIO. It's automatic operation is not good, and needs SPI enabled/disable across the transaction.
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
‎2025-05-07 9:59 AM - edited ‎2025-05-07 10:00 AM
hmmm... my SPI_Init() has CS as software driven. I'll clock through with the scope & debugger tomorrow. I must be setting it somewhere between byte Tx's.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-08 1:52 AM - edited ‎2025-05-08 1:54 AM
Frustratingly the SPI call backs dont work in the debugger so they just hang which doesn't happen when its just running.
Anyway, it looks like I have no control over the CS line (PA4). When I clock through the code in the debugger & get to the line,
HAL_GPIO_WritePin(ADXL_GPIO_Port, ADXLCS_Pin, GPIO_PIN_RESET);
The trace on that pin stays HI only when,
HAL_SPI_Transmit_DMA(adxlParams.hspi, command_address, 2);
is called does the CS line get pulled LO & then it exhibits the behaviour above, i.e. the CS line goes HI between each byte sent. I cant find anywhere in the HAL_SPI_Transmit_DMA() function that is acting on PA4, so that's puzzling.
So I've tried to just toggle PA4 in main() in the while() loop
HAL_GPIO_WritePin(ADXLCS_GPIO_Port, ADXLCS_Pin, GPIO_PIN_RESET);
HAL_Delay(500);
HAL_GPIO_WritePin(ADXLCS_GPIO_Port, ADXLCS_Pin, GPIO_PIN_SET);
It just stays HI
// Pin & GPIO port defines in ADXL362.h
#define ADXLCS_Pin PIN_4
#define ADXLCS_GPIO_Port GPIOA
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-08 3:31 AM - edited ‎2025-05-08 3:31 AM
Found it!!
I had configured PA4 as SPI1_NSS as soon as I reconfigured it as a GPIO output it all worked fine.
Thanks fellas for walking me through the debugging of this.

- « Previous
-
- 1
- 2
- Next »