2004-06-23 5:25 PM
2004-06-21 10:36 PM
Hi,
I'm trying to generate code in a cheap ST7LITE09 with 3 sofware PWM's. But it doesn't work and i can't find the mistake. Any idea's. This is the code: #include ''Io7FLite0.h'' // ST7Flite0 memory and registers mapping #include ''lib_bits.h'' // Predifined libraries working at bit level #include ''bitdef.h'' // This file defines the names of the bits int tijd,teller; int pwm1,pwm2,pwm3; void main(void) { LTCSR=0x10; ATCSR=0x12; PBDDR=0x07; PBOR=0x07; PBDR=0x00; teller = 0; pwm1 = 125; // write testvalue into pwm (50% dutycycle) pwm2 = 125; pwm3 = 125; _asm(''rim''); while(0) { } } @interrupt void AR_timer(void) { if (teller == 0) { SetBit(PBDR,0); SetBit(PBDR,1); SetBit(PBDR,2); } if (teller == pwm1) ClrBit(PBDR,0); if (teller == pwm2) ClrBit(PBDR,1); if (teller == pwm3) ClrBit(PBDR,2); teller++; tijd = ATCSR; // Reset timer flag } Thanks in advance!2004-06-22 1:14 AM
Below is a simple 3 channel pwm - freq 192Hz 0-100Duty.
Alter the g_cCounter reload value to adjust resolution/speed, eg. change reload g_cCounter with 20 will alter pwm freq to approx 960Hz, the resolution will be much less - 20 steps rather than 100. Adjust to suit your project. unsigned char g_cCounter; counter for motor pwm volatile unsigned char g_cPwms[3]; // Motor PWM speeds void main(void) { g_cPwms[0] = 50; g_cPwms[1] = 30; g_cPwms[2] = 50; g_cCounter = 0; ATR = 0xE5F; ATCSR = 0x12; PBDDR=0x07; PBOR=0x07; PBDR=0x00; rim(); while(1); } @interrupt void AR_timer(void) { if( g_cCounter >= g_cPwms[0] ) ClrBit( PBDR, 0 ); else SetBit( PBDR, 0 ); if( g_cCounter >= g_cPwms[1] ) ClrBit( PBDR, 1 ); else SetBit( PBDR, 1 ); if( g_cCounter >= g_cPwms[2] ) ClrBit( PBDR, 2 ); else SetBit( PBDR, 2 ); if( ++g_cCounter >= 100 ) g_cCounter = 0; ATCSR; // clear OVF flag } One point to remember as this device does not have nested interrupts, the ar timer interrupt is low priority - any other interrupt will seriously interfere with the software pwm above. Regards sjo[ This message was edited by: sjo on 22-06-2004 13:49 ]2004-06-22 3:23 AM
one important difference between sjo's code and yours (although I'm not sure that's where your problem is coming from) is the use of the ''volatile'' keyword. More details at http://www.stmcu.com/forums-cat-1665-1.html
Regards, Luca [ This message was edited by: _luca on 22-06-2004 15:53 ]2004-06-22 8:44 PM
Hi,
I have changed my code in the interrupt module to the code Sjo gave, and it works! I think the problem was that when i write 'teller++' and teller = 255, it does not become 0 (as i thought), but it stays I'm not sure this is the cause of the trouble, but i'll experiment with it when i have more time. Thanks for your help!!!2004-06-23 5:25 PM
sjo,
If I want to make the PWM frequency higher to 10K/20K, if your software can do this? best regards mcuinterest