2004-12-19 12:47 AM
2011-05-17 3:03 AM
Hello Everyone,
I'm willing to use my uPSD chip to check li-on battery voltage. The uPSD suppose to alarm when the li-on battery voltage drops under 3.3V. The uPSD manual claims that A/D input voltage should be less or equal to 3.6V. In case I will connect the A/D to voltage between 4.1V and 3.6V, how it will behave? Will I receive dummy data? No data at all? Can this operation harm the device? Thanks for help.2011-05-17 3:03 AM
Hi,
you should not exceed VREF of the ADC! Otherwise the device will be damaged. Greetings, Stefan