cancel
Showing results for 
Search instead for 
Did you mean: 

problem with 36 Mhz cristal

info44
Associate II
Posted on March 19, 2003 at 12:14

problem with 36 Mhz cristal

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
info44
Associate II
Posted on May 17, 2011 at 11:53

I've drawn a card around the upsd3434a at 36 Mhz. I try first with a 12Mhz cristal with 2 capacitor (10pF) and it works well. It works well also with a 24Mhz cristal. But with a 36 Mhz there is no oscillation (I use also 10pF capacitors) ? Does I need to use a cristal resonator like on the DK3200 kit ?

Thanks,

Sebastien
yu-jun
Associate II
Posted on May 17, 2011 at 11:53

Which voltage do you use?

info44
Associate II
Posted on May 17, 2011 at 11:53

I've find the problem, I've got a complete bottle of 36mhz cristal who doesn't work.

Thanks
info44
Associate II
Posted on May 17, 2011 at 11:53

In fact there is an another problem with high speed quartz : current 36 Mhz cristal use the third overtone so it result a oscillation rate at one-third the desired speed so 12 Mhz. It's necessary to use a 36 Mhz cristal in is fundamental mode.