cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with ST7LITE0 interrupt

vincent239955_stm1
Associate II
Posted on June 20, 2005 at 08:51

Problem with ST7LITE0 interrupt

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
vincent239955_stm1
Associate II
Posted on June 20, 2005 at 00:23

Hi,

I have a problem working on LITE0 LT timer interrupt.

I had compiled a simple program and it works initially.

The timer is able to interrupt and service the routine.

However, it is unable to return to the main routine after the interrupt.

What could have been the problem?

I have attached my main.c and vector.c

Rgds,

Nick

________________

Attachments :

program.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0CE&d=%2Fa%2F0X0000000bV6%2F4F4eVaO_.2lmtWLIjpBNJf9kjz9WZRKfSLh3FHDSAEY&asPdf=false
luca239955_st
Associate III
Posted on June 20, 2005 at 06:54

change

void Timebase_1mS(void)

with

@interrupt void Timebase_1mS(void)

Regards,

Luca (Cosmic)

wolfgang2399
Associate II
Posted on June 20, 2005 at 08:51

Hi Nick,

by the way: if you are using a Metrowerks compiler you have to declare your routine as interrupt-routine with the #pragma directive

#pragma TRAP_PROC (or #pragma TRAP_PROC SAVE_REGS)

void Timebase_1mS(void)

......

In addition:

Parts of the vector table should be of the type

void (*NAME)(void) .

Wonder what the casting operator of the compiler does with a ''0'' in the vector table....

Another thing:

Be careful with comments in a #define directive. Because e.g.

#define RIM _asm('' rim'') //comment

will substitute the string ''RIM;'' for

_asm('' rim'') //comment;

that means the '';'' will be ineffective after substitution.

Better you use the comment with /* ... */ e.g.

#define RIM _asm('' rim'') /* comment */

or strictly abstain from using comments in #define directives.

Regards

WoRo