2005-09-15 8:53 PM
2005-09-15 8:53 PM
hello everyone,
I got stpc atlas evaluvation kit. And i used primary loader and secondary loader downloaded from the stpc site. my problem is, as per the document i should load my secondary loader at 80000h. when i did so it did not come. only my primary loader came up (this i saw thru the printouts from serial port). After several test, this is my working condition, My secondary loader is at c0000h. I have to disable all cache and run it in the protected mode. In 80000h when i enable cache(L1) the data at 80000h is wrong. but when i disable the data is correct but not executing. Can any one tell what is there between cache and 80000h location. Wether my cache (l1) can be tested