2023-10-05 10:16 PM
Hello, can u suggest any part number which has specification with Allegro: A89307KETSR-J IC.
As i want to design Software less BLDC FOC single shunt motor control solution.
See the requirement as bellow,
Operating temperature range: -40C to +100C
Operating voltage range (full performance): 10V to 16V
Leakage current (25C) max. 100uA
AEC-Q components
2023-10-30 3:58 PM
This forum thread was marked by the moderator as needing a little more investigation, so a Support case was created in your name and will be handled off-line.