2007-09-25 2:14 AM
2007-09-11 10:56 AM
Hi all,
I´m working with Cosmic CxST7 version 4.5.5 and I´ve got the message below: Running ST7 linker clnk -l''C:\Program Files\COSMIC\CXST7_16K\Lib'' -o Debug\sugar_project.st7 -mDebug\sugar_project.map Debug\sugar_project.lkf #error clnk Debug\sugar_project.lkf:1 function _SetEP0TxStatus is reentrant #error clnk Debug\sugar_project.lkf:1 function _SetEP0RxStatus is reentrant After change the memory model to Long Stack this problem was fixed but a new one was prompted: Running ST7 linker clnk -l''C:\Program Files\COSMIC\CXST7_16K\Lib'' -o Debug\sugar_project.st7 -mDebug\sugar_project.map Debug\sugar_project.lkf #error clnk Debug\sugar_project.lkf:1 segment .bss size overflow (41) The command: ''clnk -l''C:\Program Files\COSMIC\CXST7_16K\Lib'' -o Debug\sugar_project.st7 -mDebug\sugar_project.map Debug\sugar_project.lkf '' has failed, the returned value is: 1 exit code=1. It seems that RAM space from 0x180 to 0x23f (ST72F63BK4) is not enough for application. My first question is: after modify memory model to Long Stack is it necessary to change functions to @stack rather than @nostack declaration? In Cosmic manual it is recommended select the memory model based on some procedures. After compile in long memory model settings, it´s necessary to check map file to further clues. Actually, I stuck at the second step as the compiler didn´t generate the map file. What is possible to do with the compiler settings in order to fix the problem? I´ve already attempted several ways but unfortunatelly with no sucess. Thank you very much in advance, Wilson2007-09-11 10:35 PM
2007-09-12 3:50 AM
Thanks Luca,
I´m working on this issue right now. In addition, is there any documment declaring type objects size? Actually I´ve only found descriptions for short int and long int that are, respectivelly, two and four bytes long. I wonder to see a documment depicting the rest of the types objects. Any hint for this thread? Regards, Wilson2007-09-25 2:14 AM