cancel
Showing results for 
Search instead for 
Did you mean: 

Meaning of P25C256F SPI EEPROM "write time"?

Pje
Associate III

Hi All,

I want to ask a general question regarding EEPROM with SPI Interface,

I am not sure if I understand the Datasheet correctly however it mentions that I can clock in 64 bytes (with the CS line pulled Low) then it mention the EEPROM has a write time of aprox 5mSec my confusion  is this  5mSec write time after I pulled the CS High which is after the last byte .

In general do I clock in the 64 bytes then pull the CS high and then the EEPROM writes the Data or should I keep the CS low for 5mSec after the last byte before pulling it high again .

At the moment I Pull CS High after the last byte and wait approx 6mSec ,I see all the data I write on my LA and when I read they are resonably in the expected positions (addresses ) however ther are a problem in 2 pages with wong values in the addresses although the write data log on the LA show that the bytes are written corrcetly and the page addreses are also  correct,

I appreciate any hints or help as allways.

it is P25C256F EEPROM 

 

Regards Pje

 

1 ACCEPTED SOLUTION

Accepted Solutions
Mike_ST
ST Employee

Hello,

It is not our product, but:

in the V1.3 datasheet page 19 (look for "tW" token):

"Driving the Chip Select (S#) signal high at a byte boundary of the input data triggers the self-timed Write cycle
that takes tW to complete (as specified in AC tables in: DC and AC parameters)."

View solution in original post

3 REPLIES 3

@Pje wrote:

I am not sure if I understand the Datasheet correctly


You need to take that up with the manufacturer to confirm what, specifically, they mean!

It's not an ST part - is it?

Is it the same as this one https://community.st.com/t5/stm32-mcus-products/eeprom-help-needed/td-p/740205 ?

Mike_ST
ST Employee

Hello,

It is not our product, but:

in the V1.3 datasheet page 19 (look for "tW" token):

"Driving the Chip Select (S#) signal high at a byte boundary of the input data triggers the self-timed Write cycle
that takes tW to complete (as specified in AC tables in: DC and AC parameters)."

Pje
Associate III

Hello Mike,

Thank you for your kind help,yes I do understand and did so when I post the question that it is not an ST product and that being the reason why I stated a general question,There are many people around this forum that has a great deal of general knowledge and which are kind enough to help other regardless of the Product manufacture , after all we all use ST MCU's to interface with all sorts of other components :) 

I appreciate your help in clearing my confusion ,

Regards 

Pje