2025-01-09 11:58 PM
Does the M95M04-A145 chip support data erasure at 145℃?
Solved! Go to Solution.
2025-01-10 12:15 AM
Welcome @suuulx, to the community!
Yes, you can erase the M95M04-A145 at max 145°C. However, please bear in mind that this is the maximum temperature and affects the write cycle endurance, which is then only 100k cycles (see data sheet, table 8).
Regards
/Peter
2025-01-10 12:15 AM
Welcome @suuulx, to the community!
Yes, you can erase the M95M04-A145 at max 145°C. However, please bear in mind that this is the maximum temperature and affects the write cycle endurance, which is then only 100k cycles (see data sheet, table 8).
Regards
/Peter
2025-01-12 4:48 PM
Thanks!