2008-09-08 1:13 AM
2008-09-08 1:13 AM
Hello everybody,
I have a problem concerning the Loopback function of the UART1 of the Str71. If I enable this function I cannot receive data (from an external device) anymore. If I disable it the reception of data works properly. Please have a look at the sample code below. Thank you Jojo uart1.disableLoopBack( false);// if this is set to ''true'' I get a timeout in the receiveData function (see below) uart1.enableSmartCardInterface(); uart1.clearRxBuffer(); uart1.clearTxBuffer(); uart1.enableReceiver( true ); uart1.enableFifos( true ); uart1.setGuardTime( 2 ); uart1.setBaudRate( 9600 ); uart1.setEvenParity(); uart1.setStopBits( STOP_BITS_1_5 ); uart1.setDataMode( MODE_8BIT_DATA_PARITY ); uart1.enableUart(); uart1.clearRxBuffer(); reset();//triggers the data sending to the microcontroller uart1.clearRxBuffer(); lengthATRTable=ATRLENGTH; if(!receiveData(atrTable, &lengthATRTable, TIMEOUT)) [...] bool receiveData(unsigned char *recBuffer, unsigned long *lengthRecBuffer, const unsigned long timeout) { unsigned long timeoutCounter=0; unsigned long recCounter=0; uart1.enableReceiver(true); while((!(uart1.isRxBufferNotEmpty()))&&(timeoutCounter { timeoutCounter++; } if(timeoutCounter { for(long i=0;i if(uart1.receiveByte(&recChar, 0xff)) { recBuffer[recCounter]=(unsigned char) recChar; recCounter++; } } (*lengthRecBuffer)=recCounter; return true; } [....] }