2004-10-18 2:25 PM
2011-05-17 3:03 AM
Hello,
The uPSD33XX has tow IrDA UART modes. The IRDACON Register Bit Definition at address CEH bit 6 = 1 selects the IrDA mode. Address CEH bit 5 is the IrDA Pulse Modulation Select: 0 = 1.627µs 1 = 3/16 bit time pulses May I get the timing diagram for that tow modes. The timing in the uPSD33XX is not looking correct. Regards,2011-05-17 3:03 AM
See attached bmp file.