2007-08-26 10:11 PM
2007-07-02 1:58 AM
Hi all,
I have a problem with IT interrupt. I configure pin PA7/IT4 as falling edg interrupt. ---> ITRFRE = 0x40; when i get falling edg on pin PA4 the software jump to INT_IT1IT8 interrupt routine till here evrything fine. the problem is: if i get another falling edg on PA4 when the software is already in the INT_IT1IT8 interrupt routine the sofware jump again to INT_IT1IT8 after the software get out from the INT_IT1IT8 of the first falling edg. How can i clear the pending bit of the interrupt??? i tried to disable the interrupt at the beginning of the INT_IT1IT8 and enable it at the end of the INT_IT1IT8, but it didn't help. Thanks in advance.2007-07-02 2:02 AM
I forgot to mention thet i work with ST7260 microcontroller
Thanks.2007-08-26 10:11 PM
Hello,
I have the same problem. Is there someone to help us ? Thanks