2023-07-27 6:57 PM
I’m trying to get streaming data from the following combination:
- Device: STHS34PF80
- Adaptor: MKI231KA
- Motherboard: STEVAL-MKI109V3
I’ve connected a terminal emulator (PuTTY) to the USB port and can connect.
I can type the following commands:
*setdb231KA (yellow light comes on)
*zoff
*odr06, which presumably gives me a 8 Hz ODR (I’m not sure if this is the way to write to the register)
* start
Nothing happens.
I know I’m communicating because:
*dev returns STHS34PF80
*ver returns V3.42.4
*board returns ProfiMEMSTool
I’ve read through:
- DS13916 STHS34PF80 Datasheet
- UM2116 STEVAL-MKI109V3 Professional MEMSTool motherboard for MEMS adaptor boards
- DB4783 STEVAL-MK1231KA Data brief
- AN5867 Application Note
Still don’t know what to do.
Can anyone give me the series of commands to stream the infrared-intensity data to the terminal emulator? From there I can write an application to detect swiping.
2023-09-14 1:29 PM
Hello @SophieA ,
There has been a case created to resolve this question and we will be reaching out to you directly.
Regards,
Roger