2003-10-21 11:13 AM
In-System JTAG Debugger for uPSD32xx
2011-05-17 02:56 AM
Hello!
Another question concerning uPSD. I have the information from 3rd party developing company, that ST was to produce a JTAG debugger which costs only 100-200$. This part was proposed to use the same Flash-link interface as it uses now for ISP. Will you answer, when is this part is availible? Thank you very much in advance.2011-05-17 02:56 AM
Yes, ST and Keil developed a JTAG debugger called ULINK (under $200), however, it is for debugging the Turbo uPSD 33xx family processors. You can find more information on ULink at:
. As far as for uPSD32xx family, you can obtain emulator from Nohau, which is more pricy but works very well, or you can use a lower cost emulator from Manley ~$200 but some of the fuctions are not yet supported, such as memory tracing and memory paging. You can get additional information on Manley ME3200 at: