cancel
Showing results for 
Search instead for 
Did you mean: 

USB Functions

lrodrigues
Associate II
Posted on October 21, 2003 at 09:43

USB Functions

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
lrodrigues
Associate II
Posted on May 17, 2011 at 11:56

Hello all…

I don’t have so much experience with the C language and the USB protocol, and I need to utilize the routines for transmit/receive by this protocol, these routines are in the DK3200_dsn_2.zip archive. I have some doubts about the functions implemented in this archive. The questions are:

- What I have to set (variables, SFRs…) and which functions are necessary to call for transmit a data by USB?

- When I will know that I can transmit data by USB (USB is not in busy)?

- When I will have sure that the transfer or reception has been finished?

- Where are the data received and where I will put the data for transfer?

- Which are the differences between the SFRs UDT0 and UDT1?

These questions can be simple, but I couldn’t resolve than.

If somebody has a good tip about USB I would like to know.

Excuse for the used grammar.

Regards.

Witt