2019-02-04 9:59 PM - last edited on 2023-07-21 1:57 AM by Amel NASRI
To reproduce
#define configUSE_I2C 1
gnssMsg = GNSS_Get_Buffer(&pGNSS);
UART default setting works fine.
2019-03-13 4:15 AM
Hi
Nucleo-L073RZ is one of the platform tested.
It's strange you don't have it working.
Do you see the red-led blinking on X-Nucleo-GNSS1A1?
If not the X-Nucleo is under reset and you have De-Reset it.
In the X-CUBE-GNSS1 there are already prebuilded binary also for Nucleo-L073RZ. Could you test it?
Thanks
Regards
Francesco
2019-03-13 6:47 AM
Hi
I can confirm what stated by Francesco. Nucleo-L073RZ is supported and working for both configurations (UART and I2C). Are you testing the latest released version X-CUBE-GNSS1A1 V2.1.0?
Regards
Andrea