2006-05-24 4:30 PM
2006-05-24 4:30 PM
Could some experts in this forum kindly
take a look at my I2C routines below. The problems are: config_I2C1() ..... not sure if this correct write_I2C_configuration_PCA9555() ..... write the wrong value !!! read_I2C_PCA9555() ..... my system hang as soon as the function is called !!! Here is the code: //////////////////////////////////////////////////////////////////////// void config_I2C1(void) { GPIO_Config(GPIO0, I2C_SCL|I2C_SDA, GPIO_AF_OD); //Open-drain output for SCL (P0.2), SDA (P0.3) I2C_Init(I2C1); //Initialize I2C1 I2C_FCLKConfig(I2C1); //Config I2C freq. according for FCLK freq. I2C_OnOffConfig(I2C1, ENABLE); //Enable I2C Peripheral I2C_SpeedConfig(I2C1,90000); //Select I2C Clock speed = 100khz I2C_AcknowledgeConfig(I2C1, ENABLE); //Enable Acknowledge feature } ///======================================================// void write_I2C_configuration_PCA9555(void) // Set both PORTS as INPUT --- Send 4-bytes { I2C_STARTGenerate(I2C1, ENABLE); //start condition while (I2C_FlagStatus (I2C1,DIRECT,I2C_SB) == RESET); //Check Start bit Flag I2C_AddressSend(I2C1, 0x40, I2C_Mode7, I2C_TX); //Send PCA9555 ADX Write = 0x40 while (I2C_FlagStatus (I2C1,DIRECT,I2C_ENDAD) == RESET); //Check End-of-address xmit I2C_FlagClear(I2C1, I2C_ENDAD); //Clear Flag I2C_ByteSend(I2C1, 0x06); //Send CMD 0x06 -- Port Configuration while (I2C_FlagStatus (I2C1,DIRECT,I2C_BTF) == RESET); //Check byte-transfer-finish flag I2C_ByteSend(I2C1, 0xff); //Send 0xff -- Set Port0 as Input while (I2C_FlagStatus (I2C1,DIRECT,I2C_BTF) == RESET); //Check byte-transfer-finish flag I2C_ByteSend(I2C1, 0xff); //Send 0xff --Set Port1 as Input while (I2C_FlagStatus (I2C1,DIRECT,I2C_BTF) == RESET); //Check byte-transfer-finish flag I2C_STOPGenerate(I2C1,ENABLE); //Stop Condition } ////=====================================================// void read_I2C_PCA9555(void) { I2C_STARTGenerate(I2C1, ENABLE); //start condition while (I2C_FlagStatus (I2C1,DIRECT,I2C_SB) == RESET); I2C_AddressSend(I2C1, 0x40, I2C_Mode7, I2C_TX); //Send PCA9555 ADX Write = 0x40 while (I2C_FlagStatus (I2C1,DIRECT,I2C_ENDAD) == RESET); I2C_FlagClear(I2C1, I2C_ENDAD); I2C_ByteSend(I2C1, 0x00); //Send CMD 0x00 -- Port0 Input Register while (I2C_FlagStatus (I2C1,DIRECT,I2C_BTF) == RESET); I2C_STARTGenerate(I2C1, ENABLE); //Re-start condition while (I2C_FlagStatus (I2C1,DIRECT,I2C_SB) == RESET); I2C_AddressSend(I2C1, 0x41, I2C_Mode7, I2C_RX); //Send PCA9555 ADX Read = 0x41 while (I2C_FlagStatus (I2C1,DIRECT,I2C_ENDAD) == RESET); I2C_FlagClear(I2C1, I2C_ENDAD); PCA9555_port0 = I2C_ByteReceive(I2C1); //Receive 1st Byte (Port0 of PCA9555) PCA9555_port1 = I2C_ByteReceive(I2C1); //Receive 2nd Byte (Port1 of PCA9555) I2C_AcknowledgeConfig(I2C1, DISABLE); //none-ACK I2C_STOPGenerate(I2C1,ENABLE); //Stop Condition ///========================================================//