2005-03-06 9:39 PM
2005-03-04 2:17 AM
Could anyone provide some example code using the BSPI sending bytes at ''full speed''.
The application notes dealing with BSPI is using a delay() function in between each byte sent. There must be some way to monitor some status bit in CR2. I'm interested in an example of sending data without using the transmit FIFO. An example using the transmit FIFO and an interrupt when the FIFO needs to be refilled would also be OK. thankyou, Zamid