2005-06-01 7:50 PM
2005-05-30 7:57 PM
It seems that ST7VP do not support progarmming ST72F63BK6. Is there any new version software ?
Tks2005-05-31 2:45 AM
The Engineering Programming Board ST7MDTU3-EPB is supported by STVP7 r1.9.4. With it you can program the ST72F63BK6 device.
[ This message was edited by: Alaini on 06-06-2005 10:17 ]2005-05-31 10:01 AM
Or if you want to build a programmer try Flashbash - www.spen-soft.co.uk
Regards sjo2005-05-31 6:53 PM
The ST7MDTU3-EPB do support the socket, however, the ST7VP version 1.9.3. OCT 27,2004 only support to ST72F63BK4; Is there any new version S.W(ST7VP)?
Tks!2005-06-01 6:26 PM
Jackie,
The new version of STVP7 will support the ST72F63BK6 device. It will be released in 1 or 2 months. However, if your software is less than 16 K, then you can program the device by selecting BK4. Pls make sure that the firmware lies in memory 0x8000 to 0xffff in this case. Regards.2005-06-01 7:50 PM
Get it! Tks!