2004-08-27 3:50 AM
how to config the ports of MCU module?
2011-05-17 3:02 AM
Hi!
In the PSDsoft express, the ports of MCU module must be configed in some mode, such like txd or rxd,but in the software , the initialization of uart is also needed. I want to know if the pins of MCU module are not defined in PSDSoft express, but it is initialised in the software, can these pins work fine ? Thanks!2011-05-17 3:02 AM
In uPSD32XX the alternate functions can be set up either by writing to registers at runtime, or by PSDsoft express. Some can only be set by writing to registers.