cancel
Showing results for 
Search instead for 
Did you mean: 

psd soft problem

sjo
Associate II
Posted on August 23, 2004 at 09:46

psd soft problem

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
sjo
Associate II
Posted on May 17, 2011 at 12:02

I am implementing a iap bootloader, all is going ok with the actual code but I have noticed a strange problem with PSDExpress v8.10.

If I try and implement the memory map below psdexpress will change fs0(page0) to 0-ffff instead of 8000-ffff. If I change fs0 to 0-6fff (instead of 7fff) everything is ok.

The simple idea is boot into secondary flash, validate primary flash then perform a switch. page0 is only selected during flash programming to move out of sram memory space.

fs0 0x0000 0x7FFF

fs0(page0) 0x8000 0xFFFF

fs1(page1) 0x8000 0xFFFF

fs2(page2) 0x8000 0xFFFF

fs3(page3) 0x8000 0xFFFF

fs4(page4) 0x8000 0xFFFF

fs5(page5) 0x8000 0xFFFF

fs6(page6) 0x8000 0xFFFF

fs7(page7) 0x8000 0xFFFF

csboot0 0x0000 0x1FFF - iap bootloader

csboot1 0x2000 0x3FFF - iap bootloader

csboot2 0xC000 0xDFFF - eeprom emulation

csboot3 0xE000 0xFFFF - eeprom emulation

rs0 0x4000 0x5FFF

csiop 0x0200 0x02FF

Is it me or is this a feature ?

I have attached psdexpress project.

Regards

sjo