2023-04-03 3:34 AM
2023-04-03 4:29 AM
Welcome, @NVall.2, to the community!
The EVALSTPM3X-3PH, a poly-phase evaluation board, was a Class 0.2, single-phase or poly-phase
meter with current transformer sensors.
I regret to inform you that the board has already been discontinued, so no more information is available from STMicroelectronics. Furthermore, it was based on an STM8S903K3, which was already set to NRND (Not Recommended for New Designs).
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-04-03 4:29 AM
Welcome, @NVall.2, to the community!
The EVALSTPM3X-3PH, a poly-phase evaluation board, was a Class 0.2, single-phase or poly-phase
meter with current transformer sensors.
I regret to inform you that the board has already been discontinued, so no more information is available from STMicroelectronics. Furthermore, it was based on an STM8S903K3, which was already set to NRND (Not Recommended for New Designs).
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter