cancel
Showing results for 
Search instead for 
Did you mean: 

Can you help me to obtain the datasheet of component S102338002C ?

STshi.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

For customised devices, i.e. components that a specific customer only has manufactured for him, a data sheet is also only available for this customer. Logically, it is not available for other customers; after discontinuation, all documents were destroyed anyway.

Now one could speculate where the Asian seller probably got these devices, but that doesn't help anyone. In any case, it is a bad idea to buy components of which you do not have the documentation beforehand.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

It is with great regret that I have to inform you that no documentation is available for this. You should contact the respective seller, who should have information on his components - if it is a serious one.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
STshi.1
Associate

Thanks for your reply. The S102338002C is an semiconductor in a TO-220-7 package. It is esteemed to be a dual MOSFET component seen from the circuit in which it was found. This component is out of production and no longer available through the regular distributors. I have a suspicion that this part was custom designed in a limited production. I managed to buy a few from a chinese supplier but he can't deliver the datasheet nor do other vendors. Since the component is produced by ST, a datasheet must be available somewhere within ST. Hence my question to ST.

For customised devices, i.e. components that a specific customer only has manufactured for him, a data sheet is also only available for this customer. Logically, it is not available for other customers; after discontinuation, all documents were destroyed anyway.

Now one could speculate where the Asian seller probably got these devices, but that doesn't help anyone. In any case, it is a bad idea to buy components of which you do not have the documentation beforehand.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.