2003-05-18 10:13 PM
2003-05-16 2:24 AM
Hello all,
I have a question: what is the purpose of the floating interrupt input and how can I use them? Thanks for your help.2003-05-18 10:08 PM
Hi Thilo,
the floating interrupt input is usefull if your signal which is generating this interrupt is for example a TTL of CMOS signal. In that case you don't need an internal pull-up resistor. An internal pull-up would cause an additionl current consumption if the external signal is low. Especially during a low-power mode this extra current should be avoided. Rolf2003-05-18 10:13 PM
This give you the option to use a pullup/down resistor of your choice rather than using the builtin pullup resistor.
Regards SJO