2004-08-09 5:57 AM
2011-05-17 3:02 AM
Hello,
i was using UPSD3234A on my old project and use flashlink.I use the same programming interface (pullup resistors, serial resistors etc.)as DK3200 board (it has 5V technology) and now i will use UPSD3254BV that works with 3.3V. Will be there any differences that i must apply with programming interface to use flashlink to program UPSD3254BV. Regards2011-05-17 3:02 AM
FlashLink works with both 5.0V and 3.3V devices (it is specified for operation from 2.7 to 5.5V). Pull-up resistors connected to 5V on the 5V version will be connected to 3.3V on the 3.3V version of the device. The hardware interface is the same.