2008-02-08 1:08 AM
2011-05-17 12:49 AM
/*
I have written an application that sits in bank 0, and have a bios sector in bank 1. I have not been able to get a function I've written to work that, I hope, will allow me to switch banks and run my bios routine in bank 1. I can see from the Segger J-Flash utility, that my program is indeed there in bank 1, but I can't switch to it. Sending a ''0'' to this function resets the processor, and sending a ''1'' makes the processor hang, and only gets out of being hung by power cycling the board. I am close to having a firmware download routine working, but am unable to get this part working. There is something simple I must be missing..Any help would be greatly appreciated. Here is my routine: My application starts at address 0x0, and the bios sector starts at 0x80000. I'm using the IAR4.41A compiler, and am using the STR912FAW44 version of the chip. */ typedef void (*pfunc)(void); __ramfunc void bankSwitch(char bankNo) { pfunc jump2App; if(bankNo){ FMI_BankRemapConfig(4,2,0,0x80000); }else{ FMI_BankRemapConfig(0,6,0x80000,0); } jump2App = (pfunc)0x0; jump2App(); } [ This message was edited by: jmullens on 12-02-2008 03:35 ]2011-05-17 12:49 AM
Hi,
Segger offers a free tool(JlinkSTR91x.exe) allowing: erase all flash protect sector switch boot bank ..... The following link(segger forum) explains how to use this tool: http://www.segger2.com/index.php?page=Thread&threadID=22 Rgds,