2006-01-26 12:21 AM
field firmware update & serial Port
2006-01-08 8:57 PM
I found appnote AN2078 STR71x In-Application Programming using UART.
''The maximum size of the image to be loaded: 56 Kbytes.'' meaning STR712FR2 (code 256 KB) can be program up to 56Kbyte?,buy STR712FR1 (code 128 KB) is better ? [ This message was edited by: kmaster on 09-01-2006 10:31 ]2006-01-08 9:13 PM
Hello,
In fact this application note will be updated in next few weeks. The new version of the AN2078 will allows the user to program all the 256KB. I think to by an STR712FR2 or an STR712FR1 does not depends on the AN2078 but depends on the user application resources. Because the AN2078 is an application note, not a bootloader, and the user has to load the application note code using a specified flasher tool then run it. Thanks. [ This message was edited by: Bouha on 09-01-2006 10:46 ]2006-01-08 9:44 PM
First production will use STR712FR2 and install IAP/bootloader via JTAG.
In field (After sale service) will programming via PC-RS232. Waiting for new IAP(AN2078)... [ This message was edited by: kmaster on 09-01-2006 11:17 ]2006-01-09 1:18 AM
Is AN2078 also available for the IAR compiler?
THX Bertl2006-01-09 3:03 AM
Actually the AN2078 is available for RVDK toolset.
Thanks2006-01-16 2:52 PM
How long to launch new version (New-IAP program all flash) ??
Can be use JTAG-wiggler to program STR712FR2 ??2006-01-16 7:45 PM
A new version is planned to be published on STMCU website in week 7.
Find attached a beta version of this application note which is under validation. Please Let me know if there is something wrong 8-) ________________ Attachments : IAP_V2.0.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtEE&d=%2Fa%2F0X0000000aKX%2F9qoG2lRxbBMi_.JsMqlVg_6QdSRkAnwhbBAf_qmM9xw&asPdf=false2006-01-16 11:10 PM
ST have a future product (STR7xx) that support On-Chip bootloader (like P89C51RD2 ) ??
User can program via JTAG or UART0 available for low price programmer. Commercial JTAG $100-$1000, RS232(UART0) $5.2006-01-17 7:08 PM
For more information about the STR7xx products, contact your nearest distributor or ST sales office.