Posted on March 30, 2006 at 04:34I'd like to use the last 3 bytes of the flash memory to identify if there's a valid program in the flash. How can I read them in the scatter file instead of reading P1.8? THX, Bertl
Posted on January 09, 2006 at 12:01Hi! Did anyone as mentioned in AN2078(last page) remap his RAM to address 0x0! What does that mean? Is there an example available? And did anyone convert AN2078 source-code to IAR compiler? THX Bertl
Posted on January 05, 2006 at 09:58Did anyone work with segments to access external RAM (IAR-Compiler) and if so could you give me an example how to handle segments with the iar compiler/Linker. THX Robert