2005-06-15 11:28 PM
External clock DVP3 generates GDI Error
2005-06-13 9:36 PM
Hi, I'm using STMDT10-DVP3 and STVD7 3.1.1 to emulate ST7LITE29. When I select FOSC: EXTERNAL the following message appears on screen: ''GDI Error: [10255]''. I have an external 8MHz qrystal connected to OSC1 and OSC2. Whats wrong?
Regards bood2005-06-14 9:52 PM
Hi,
When you want to use an external clock you must connect TTL clock signal between EXTCLK pin and GND (see figure 8 of ST7DVP3 user manual attached). The development kit doesn't use the application Crystal connected on OSC1/OSC2 because flat rebbon capacitors can disturb oscillator. But if you want to use 8MHz frequency you can select it directly with menu: Debug instrument > MCU configuration > Option and chose 8MHz. With best regards, ________________ Attachments : st7dvp3.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I05s&d=%2Fa%2F0X0000000bWD%2FBZ.4JuJ3L1z1BuhX8NtFLHTAT.ImWrtvyGF9G5bp9EM&asPdf=false2005-06-15 11:28 PM
Okey, thanks!
/bood