2005-06-29 8:44 PM
2005-06-29 3:33 AM
Hi,
I work on ST10F168 with 2 * 1Mb * 8 bits SRAM on external bus. I use A1 to A20 and WRL for the first ram and WRH (P3.12/BHE) for the second. It works very good. But i would to know if i can use only one write signal for the 2 ram. For example the WR signal on the 2 chip. Because i want to connect a 16 bits sram with just one WR. Thanks in advance2005-06-29 5:16 AM
Thank you for your answer and your precision !
But i don't understand why we can't use external bus with just 1 CS, 1 RD, and 1 WR when it works in 16 bits non-multiplexed ??? Best regards