cancel
Showing results for 
Search instead for 
Did you mean: 

External 8 bits Mux RAM

jm
Associate II
Posted on October 24, 2003 at 08:07

External 8 bits Mux RAM

2 REPLIES 2
jm
Associate II
Posted on October 22, 2003 at 06:44

Hi,

I work on st10f168, and i want to connect external RAM to it using EBC

But in 8 bits MUX mode, i don't know which port is use to datas and adress.

So if you use it in the same configuration, give me a answer

THANKS a lot

bye

maxime2399
Associate II
Posted on October 24, 2003 at 08:07

The data are on port P0L and the addresses on P0, P1 and eventually P4. for more detail have a look at the ST10x167 user's manual.

(ST10R167 and ST10F168 are fully compatible except for the program memory)

http://www.stmcu.com/mcdfiles/7317.pdf