cancel
Showing results for 
Search instead for 
Did you mean: 

EVALKITST7580-1 works well in one direction and bad in other

i7im
Associate
Posted on March 25, 2014 at 14:34

I have two

EVALKITST7580-

1.

One of them

I configured

as the master

(call it

device

1).

The other

as the slave

(call it

device

2).

When I run

a

ping

gui

,

master

sends 100 and receives

100 messages.

When I make

device

1

as slave

and the

device

2

as master, master

sends 100

and receives

82-92

messages.

Then

I change

the device

places.

Again one of them

I configured

as the master

(

device

2).

The other

as the slave

(

device

1).

Master

sends 100 and receives

100 messages. And when I make

device

2

as slave

and the

device

1

as master, master

sends 100

and receives

82-92

messages.

Again

the problem

with the transmission

in one direction (

from one

corner of the room

to the other, regardless of the device

and its

roles

)

.

What happens? If this noise, they should interfere in both directions?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0