cancel
Showing results for 
Search instead for 
Did you mean: 

EOS 2.2 is released

michael
Associate II
Posted on June 20, 2008 at 06:10

EOS 2.2 is released

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
michael
Associate II
Posted on May 17, 2011 at 09:53

EOS is an open source real time kernel that was originally developed for the Infineon XC167 processor, and is freely available at

http://sourceforge.net/projects/eos-xc167-rtos

The following features were introduced in version 2.2:

* The interface 'rtos_disable_scheduler' is modified so that it prevents interrupts from causing scheduling.

* The number of utilized hardware timers is reduced from 3 to 2.

* Hardware timer frequencies are adjusted to match the required 100[µs] at 40[MHz].

This is the final release for the C166 family as my interests have shifted towards the ARM architecture.