cancel
Showing results for 
Search instead for 
Did you mean: 

Help on HItop IDE

sr_shinde
Associate II
Posted on June 26, 2008 at 02:25

Help on HItop IDE

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
margd123
Associate II
Posted on May 17, 2011 at 09:53

Hello,

to create a new project,open the Hitop.

1)in the ''using projects in Hitop'', click on create ''a new project from a template''.

2)choose your compiler and your micricontroller.

3) The project will be made with a default settings (compiler,assembler and linker), you can use this configuration.

4) add your source file and don't forget to add the path of the header files(Project->settings->tools settings->include directories).

5) to generate an elf file set the extension of the target name to .elf(from project->settings->tools settings->general->target name)

- Attached you find a preconfigured project with tasking compliler (It should be better to download the latest version of hitop-arm (5.30))

regards,

mgd.

sr_shinde
Associate II
Posted on May 17, 2011 at 09:53

HI all.Does anybody know/using HiTOP IDE then please help me.

Tell me the procedure to create new application.I face some problem with creating elf file,symbol preprocessor.I fail to generate .elf, .htx and .sym . Ide ask for elf at start only.

So, if anybody knows tell me the complete procedure to create new project , then new application, IDE configuration, compilation and linking.

Best regards

Sai

sr_shinde
Associate II
Posted on May 17, 2011 at 09:53

Thanks for reply

But didnt got any help from it.There is no option ''using projects in Hitop''

as such. Iam using HiTOP52-ARM

Version-05.20.0310

So please give me further detail.

Best regarg

sai

[ This message was edited by: sr_shinde on 24-06-2008 12:06 ]

margd123
Associate II
Posted on May 17, 2011 at 09:53

Hello,

the ''using projects in Hitop'' is a window which appears when opening Hitop.

you can find all the necessary information in the Hitop online help(in the section ''getting started->starting up the system->starting hitop''

mgd,

sr_shinde
Associate II
Posted on May 17, 2011 at 09:53

Hi

''using projects in Hitop'' window doesnt appear when i open Hitop.

i am using evaluation version

Regards