‎2009-11-12 8:51 PM
Dummy question : .axf size greater than Flash size???
‎2011-05-17 12:59 AM
Hello all,
Device = STR912 I don't understand how it works (JTAG programmation) : the flash size is 512K, and the file ''.axf'' size is 700k ?? As i'm working on a bootloader solution, I'd like to know if some informations of this file should not been downloaded in flash ?? thank you‎2011-05-17 12:59 AM
Hello all,
OK, for those who ask themselves the same question : you need to generate the .bin file from the .axf file with the fromelf.exe software provided by Keil (if using Keil) or any converter you may choose. In Project : Option --> User --> Run User program After Build/rebuild, mark #1 with : c:\keil\ARM\BIN31\fromelf.exe --bin -o FileName.bin FileName.axf This .bin file is the one to use with the bootloader. Regards‎2019-02-08 9:24 AM
That's really helped me a lot, Thanks!
‎2019-02-08 9:50 AM
Generally a great deal of symbol and debug information goes into the file so it can be quite expansive.
You can get an effective dump/disassembly via
FromELF -c -s -d foo.axf >foo.lst
‎2019-02-09 5:42 PM
yes, or
arm-none-eabi-objcopy -O binary foo.axf foo.bin
when using the arm-none-gnu-eabi toolchain:)