Skip to main content
y_gudekar
Associate III
November 24, 2008
Question

Code protection for STR912FAW44

  • November 24, 2008
  • 2 replies
  • 775 views
Posted on November 24, 2008 at 10:08

Code protection for STR912FAW44

This topic has been closed for replies.

2 replies

y_gudekar
y_gudekarAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:56

Dear All,

In one of our product i am using ST10F269.

For programming of it we are using ''code protection'' feature of it.

In this we are temporary unlocking the chip using our own tool and flash routine inside the chip. Then we reprogram the flash.

In our new product we are planning to use STR912FAW44.

For programming of same can it is possible for us to use similar technique which we are using for ST10F269?

Regards....

Yogesh Gudekar

jgoril
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:56

Hi.

You can enable Security bit during JTAG programming. Once enabled, the protection can be disabled only by full-chip erase command. See STR9 flash programming manual for details...