2006-04-16 11:40 AM
Choices of C Compilers for ST7F part?
2006-02-06 8:18 AM
I am looking at the alternatives for ST7F tools for C compiler and debug. I have a package from Cosmic. Are the any other choices? I see Metrowerks listed in web pages at Softecmicro. But I can't find much more info than this.
Are these the only two choices? - thanks, Mike2006-02-06 9:09 PM
Hi Mike,
I've never heard of any other C-Compiler for ST7 than Cosmic and Metrowerks. I use the Metrowerks and the STVD7 (visual develop) from STMicro and I am comfortable with both of them. You can download the STVD7 from thehttp://mcu.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=15
and use it for free. It is a quite practical tool. You may use the STVD7 with the Cosmic as well. Regards WoRo2006-02-06 11:32 PM
I will strongly recommend to use Cosmic in combination with STVD7 toolchain.
2006-02-08 8:18 AM
Hi Mike,
I have developed an IP stack on ST7F321 with C-Cosmic and several routine in asm with an EMU3. This emulator is very good to develop and debug complex application. I have had lot of problems with cosmic C to integrate C and ASM, especialy for routine parameter and variable declaration. Regards Sly2006-02-08 6:39 PM
Hi.
I use Cosmic since 1 year and I am satisfied. I did not have any big problems due to compiler.2006-02-08 9:59 PM
Quote:
.... I have had lot of problems with cosmic C to integrate C and ASM, especialy for routine parameter and variable declaration. What problems? Just curious. Regards, Luca (Cosmic)2006-02-08 10:04 PM
Hi Setler,
I've never had any problems with Cosmic using the STVD7 - but I don't have any after I've changed to the Metrowerks C-compiler. So why do you ''strongly recommend'' to use the Cosmic compiler??? Regards WoRo2006-02-09 7:29 AM
Hi new here, i would rather prefer STVD7
2006-04-15 5:09 AM
I will strongly recommend to use Cosmic in combination with STVD7 toolchain.
I vote at all !! I use Cosmic ''C'' compiler from about 4 years without any problem... You can believe to me ! So You can just investigate if You are using it correctly. The Cosmic support service is very efficient to help You about any problem You have. SixtusWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.