2006-04-13 2:20 AM
2006-03-21 7:19 PM
Hi all,
I'm developing a control system using ST7 & ST7538. In some cases (when power supply in not so good), the ST7538 will receive data correctly (then the register is ok) but refuses to transmit. Even after a register re-programming. I check all the lines and all works fine. Do you know if there is a tx-lock feature (other the tx-timeout one)? Do you know how the modem can be reseted? Many thanks in advance, Patrik2006-03-21 9:55 PM
Is it maybe related to UVLO (Under Voltage Lock Out) modem feature?
2006-03-23 1:25 AM
I see that after Power Good goes down for a while (Vdc falls under 4.3V) the modem will lock the transmissions (but not the receiving).
Even after Vdc returns at 5V, the modem refuses to transmit. The signal REGOK is always low (ok). Does somebody know why of this behaviour and how to restore normal operation? Thanks, Patrik2006-04-13 2:20 AM
You are right Emile :-). We only need to stop WD signal to toggle (for more than 1.5s), when PG signal falls down. This will cause, in our hw, a global system reset.
Thank you very much for your support, PatrikWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.