2024-02-15 4:53 AM - last edited on 2024-02-15 8:52 AM by mƎALLEm
Dear Ladies and Gentlemen,
for you it is your daily business - for me as customer a contemporary challenge:
Something went wrong with my pin-configuration.
I measure ~1,7 V as GPIO-output of Port A instead of wished >=3.3 V.
My power supply is a USB.
Could you give a sample pin configuration for (3.3 V output) of Port A in discussion?
As additional comment:
Round about 5 V are present at the 5 V-Pin(s).
Thank you in advance.
TIMBO
2024-02-15 10:22 AM
Sooo...
Its about DM422c - right ?
You need anyway just 3 lines : pul, dir, ena. +opto for power.
Set pins as output, open drain . PA8 , 9, 10 . + on opto 5V vom USB port .
(not PA0...123 , they are NOT FT - 5v tolerant !!! ) RTFM !!!!
2024-02-15 10:25 AM - edited 2024-02-15 1:27 PM
F U I & ((A)nswer) -
my emailaddress is ... xxx
Could you send me this answer in a more common way in german language again?
Thank's a lot ...
sou sou sou - spoken in my time ...
I would like to go on OPTO with an open common PIN as input voltage... but your solution seems to be more comfortable.
2024-02-15 10:33 AM - edited 2024-02-15 10:39 AM
>>But I need at least round about 3.6 V ... USB Voltage tap per software possible?
No, there's no magical connectivity here. Go check the schematic, the 5V goes to a 3.3V regulator powering the STM32. The STM32 doesn't have 3.6V available as a High Level
Perhaps you've damaged PA0 ? Pressed the Key, shorting out the MCU?
A photo of the PA0 voltage off the board, and not connected to anything would be more assuring.
Do you have additional BLACK PILL boards you can sanity check against?
https://stm32-base.org/assets/pdf/boards/original-schematic-STM32F411CEU6_WeAct_Black_Pill_V2.0.pdf
Provide schematics of what you've wired, over photos.
GPIOA->OSPEEDR |= 0x00000000; // Doesn't clear bits, basically does nothing
GPIOA->OTYPER |= 0xE; // PA1..3 Open Drain, then external pull-ups to 5V via 10K
A read of the DATA SHEET indicates PA0 is not FT (5V Volt Tolerant), just a standard 3.3V GPIO
https://www.st.com/en/microcontrollers-microprocessors/stm32f411ce.html
2024-02-15 11:11 AM
2024-02-15 12:52 PM
Ok - in common I think, that my control voltage is too low. The motor sounds in this way.
In look to the USB voltage, there is no possibility to get this voltage per software?
2024-02-15 12:56 PM
What actually does VB means?
Is it possible to give there a voltage input ~5V on the card?
2024-02-15 1:54 PM
>>In look to the USB voltage, there is no possibility to get this voltage per software?
How would that even work?
Have you looked at the schematics?
The D+ / D- operate at much lower voltages, and the 5V doesn't get to the STM32F4 MCU
What are you attaching? Link to a manual/datasheet for the stepper controller.
Draw a diagram of what you've connected to what. Is this too much to ask?