cancel
Showing results for 
Search instead for 
Did you mean: 

Bug report -> PLL/special interrupt mode

jens239955_stm1_st
Associate II
Posted on May 14, 2007 at 11:23

Bug report -> PLL/special interrupt mode

1 REPLY 1
jens239955_stm1_st
Associate II
Posted on May 17, 2011 at 09:43

Hi

I have tried to use RCLK divider together with the PLL at 96MHz, but cannot get to work. I use PLL @ 96MHz and RCLK/16 which gives 6MHz (ok), but if I use ''Special interrupt mode'' bit3 in PWRMNG to achieve 96MHz in interrupt rutines it does not run 96MHz. I have tried to set CLKCNTR register manually from my ISR but even though the value of CLKCNTR register has changed correctly, the speed still remains at 6MHz.

Have you experienced the same, or is it another bug?

Best regards

JL