Posted on May 17, 2011 at 09:44Hi again I have solved my problem by using ReceiveTimeoutInterrupt. I simply wired my Tx to the Rx, though I loose my full duplex it works in my application. Now I have Interrupts when I receive, and when the TxFIFO i ...
Posted on May 17, 2011 at 09:44I have the same problem with my application, and I also don't know how to solve it. If there just where a TX-complete interrupt, based on the ''Busy'' bit in flag register of the uart it would solve the problem. If I f...
Posted on May 17, 2011 at 09:43Hi I have tried to use RCLK divider together with the PLL at 96MHz, but cannot get to work. I use PLL @ 96MHz and RCLK/16 which gives 6MHz (ok), but if I use ''Special interrupt mode'' bit3 in PWRMNG to achieve 96MHz i...
Posted on May 17, 2011 at 09:42Hello ST I have tested the STR912FA with respect to power consumption and I have seen some improvement since STR912F. On the FA version I have measured 0.067mW on the core(1.8V), and 2.3mW on I/O(3.3V), but in the data...