2006-09-03 10:41 PM
Application note for converting RVDK project to IAR EWB project
2006-07-17 9:56 PM
Hi,
Does there exist some application note which tells how to port a RVDK project to IAR EWB project. All of the source code available on the site is based on RVDK. It is almost impossible to port the code on IAR Embedded WorkBench without some help. Thanks2006-09-01 11:50 AM
You can find it from the Setup dir--''C:\Program Files\IAR Systems\Embedded Workbench 4.0\ARM\doc\''
There are an Application notes---EWARM_RealViewMigrationGuide.pdf