2006-10-13 02:29 AM
2011-05-17 12:33 AM
Hello guys,
I wish to use two independent Ethernet interface with the STR912x. I was wondering if anyone made it and if yes some implementation guide will help. May i connect 2 PHY to the MII of the STR ? Thanks and have a great day.2012-05-03 11:13 PM
Hi Cofor,
I asked myself the same question, especially when both MII PHYs are on the same chip (like in the KSZ8863 from Micrel). Did you managed to find an answer? Thank you very much.