Skip to main content
Associate III
March 17, 2025
Question

Azure IOT Porting STM32H735G-DK

  • March 17, 2025
  • 0 replies
  • 462 views

Hi currently i am using STM32H735G-DK board and i need to integrate with azure IOT via ethernet 

1. From .Ioc file i have  enabled  MQTT,msns,dns,dhcp,sntp,cloud and i have added Nx azure related files and azure c sdk and the file structure as attached in the image  

2. If have referred an example in the below link and also links attached 
https://github.com/tdjastrzebski/B-L4S5I-IOT01A_AZURE-RTOS
https://github.com/STMicroelectronics/x-cube-azrtos-h7

3. The examples where all are connected with WIFI is there any example with ethernet connectivity or where i can change the things for ethernet connectivity and azure iot

4. i am using 

STM32CubeIDE

Version: 1.18.0

avinpat_8_0-1743752576150.png

avinpat_8_1-1743752608049.png

 

 

 

This topic has been closed for replies.