2004-04-07 2:23 AM
2004-04-02 2:07 AM
Hi,
I am working with the ST72F264G2 u-c (coding in asm). I would like to use a general routing to send messages via RS-232. my problem is the massage are located in the code area which is 16Bit addressing mode. Normally I would use a pointer to the message (i.e ld X,#message) and then start incrementing the address untill the message end. The problem is that X cannot get the message address. I have a lot of messages and using ''ld A,(message,X)'' for each message takes a lot of code. any ideas?2004-04-07 2:23 AM
you can use 256-Byte Pages for the messages. With
ld A,(M_BLOCK1,X) you can read the block with inc X I use the same technique for call of different programs pointed to by a PRGM_PNTR. I hope I could help you