cancel
Showing results for 
Search instead for 
Did you mean: 

Why did my LoRaWAN app only sends empty data?

Wtuya.1
Associate

I'm trying to send some GNSS data using LoRaWAN, but my gateway only receives a blank string. Pretty sure the AppData.Buffer values are right since it prints the right thing on my console.

0693W00000aIlZXQA0.pngAs you can see my gateway didn't receive any payload.

0693W00000aIlHRQA0.pngHere's my SendTxData part

    ReceiveGNSSData();
 
    hdop = (uint8_t)(GNSSParser_Data.gpgga_data.acc * 10);
 
	hour = (uint8_t)(GNSSParser_Data.gpgga_data.utc.hh);
	minute = (uint8_t)(GNSSParser_Data.gpgga_data.utc.mm);
	second = (uint8_t)(GNSSParser_Data.gpgga_data.utc.ss);
	sats = (uint8_t)(GNSSParser_Data.gpgga_data.sats);
	altitude = (int16_t)(GNSSParser_Data.gpgga_data.xyz.alt * 10);
 
 
    AppData.Buffer[i++] = AppLedStateOn;
    AppData.Buffer[i++] = (uint8_t)(hour & 0xFF);
    AppData.Buffer[i++] = (uint8_t)(minute & 0xFF);
    AppData.Buffer[i++] = (uint8_t)(second & 0xFF);
    AppData.Buffer[i++] = (uint8_t)(sats & 0xFF);
 //   AppData.Buffer[i++] = (uint8_t)((altitude >> 16) & 0xFF); ga perlu soalnya datanya cuma 16 bit jadi cukup shift 8
    AppData.Buffer[i++] = (uint8_t)((altitude >> 8) & 0xFF);
    AppData.Buffer[i++] = (uint8_t)(altitude & 0xFF);
 
    AppData.BufferSize = i;
 
    APP_LOG(TS_OFF, VLEVEL_L,
            "Send on port LORAWAN_USER_APP_PORT (%d): \r\n"
            "Led    : %s\r\n"
            "UTC    : %d:%d:%d\r\n"
            "Sats   : %d\r\n"
            "Alt    : %d.%d m\r\n",
            LORAWAN_USER_APP_PORT,
            AppData.Buffer[0] == SET ? "ON" : "OFF", // Led state
            AppData.Buffer[1], AppData.Buffer[2], AppData.Buffer[3], // UTC
            AppData.Buffer[4], // Satellites
            (AppData.Buffer[5] << 8 | AppData.Buffer[6]) / 10, // Altitude 1
            (AppData.Buffer[5] << 8 | AppData.Buffer[6]) % 10); // Altitude 2

I also attached the full lora_app if needed. Thank you.

0 REPLIES 0