cancel
Showing results for 
Search instead for 
Did you mean: 

STSAFE-A110 how to enter Hibernate

dylanou
Associate III

board: stm32U585 + stsafe-a110

before the stm32u585 enter the low power mode ,I want to set stsafe-a110 enter the low power consumpion mode.

I can't find the methods to enter Hibernate

dylanou_0-1718336059037.png

dylanou_1-1718336334937.png

dylanou_2-1718336347382.png

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Benjamin BARATTE
ST Employee

Hi @dylanou ,

 

Thanks for your interest in STSAFE-A110 solution.

The X-CUBE-SAFEA1 package offer the StSafeA_Hibernate() function to set the STSAFE-A110 in low power.

Be aware that when you are setting the STSAFE-A in hibernate mode, you have to select the wake up condition.

could be Reset pin only or (Reset pin or I2C Start condition)

In the case of wake up with I2C Start condition, be aware that any I2C communicate on the I2C bus will wake up the STSAFE-A.

To use the Reset pin, you need of course a layout that supports it.

Best Regards,

 

Benjamin

 

View solution in original post

1 REPLY 1
Benjamin BARATTE
ST Employee

Hi @dylanou ,

 

Thanks for your interest in STSAFE-A110 solution.

The X-CUBE-SAFEA1 package offer the StSafeA_Hibernate() function to set the STSAFE-A110 in low power.

Be aware that when you are setting the STSAFE-A in hibernate mode, you have to select the wake up condition.

could be Reset pin only or (Reset pin or I2C Start condition)

In the case of wake up with I2C Start condition, be aware that any I2C communicate on the I2C bus will wake up the STSAFE-A.

To use the Reset pin, you need of course a layout that supports it.

Best Regards,

 

Benjamin