2024-08-25 12:10 PM
I downloaded and installed the latest STM32Cube IDE. However, I can't compile even the simplest program, because during the creating of a project I get warning stating that I must download and install the Firmware Package.
The system is a Windows 11 virtual machine without Internet access, so I suppose I should download Firmware Package on other computer and then copy to the VM. However, I cannot locate that Firmware Package.
The problem is very similar to this one:
However that solution didn't work for me.