cancel
Showing results for 
Search instead for 
Did you mean: 

I am trying to port AC6 compiled code into Atollic True studio. But i am getting the below error, can some one help me out to build successfully. I used same STMcubeMX project to AC6 and Atollic truestudio project.

MBhar
Associate II

make clean 

Cannot run program "make": Launching failed

Error: Program "make" not found in PATH

PATH=[C:/Program Files (x86)/Atollic/TrueSTUDIO for STM32 9.0.1/ide/jre/bin/client;C:/Program Files (x86)/Atollic/TrueSTUDIO for STM32 9.0.1/ide/jre/bin;C:/Program Files (x86)/Atollic/TrueSTUDIO for STM32 9.0.1/ide/jre/lib/i386;C:\ProgramData\Oracle\Java\javapath;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Program Files\Intel\WiFi\bin\;C:\Program Files\Common Files\Intel\WirelessCommon\;C:\Program Files\PuTTY\;C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility;C:\Program Files (x86)\Atollic\TrueSTUDIO for STM32 9.0.1\ide;]

0 REPLIES 0